SLVSHR7 August 2024 TPSM8287A15M
PRODUCTION DATA
If the converter remains in regulation, the minimum required output capacitance is given by:
If the converter loop saturates, the minimum output capacitance is given by:
In this case, choose COUT(min) = 1166µF as the larger of the two values for the output capacitance.
Table 9-3 lists the output capacitors chosen. 2 × 47µF capacitors are placed close to each of the four modules, giving a minimum effective capacitance of about 27µF each. Five 220µF capacitors and five 47µF are placed near the load to approximate the total decoupling capacitance required by a typical load. Each of the 220µF capacitors yield about 138µF of effective capacitance. Together, the 1041µF of effective capacitance is very close to the required minimum value calculated above. For further calculations, use COUT = 1041µF.
Equation 50 checks that most of the output capacitance is placed at the load. If the ratio is less than 1, increase the capacitance at the load or place the device, output capacitance, and load next to each other such that there is no separation between the output capacitances.
Equation 52 calculates the output voltage ripple, based on the effective output capacitance value.
The ripple is slightly higher in the application due to the ESR and ESL in the output capacitors and the application board parasitics.