SCDS252B July 2007 – June 2021 TS5A23157-Q1
PRODUCTION DATA
SYMBOL | DESCRIPTION |
---|---|
VCOM | Voltage at COM |
VNC | Voltage at NC |
VNO | Voltage at NO |
ron | Resistance between COM and NC or COM and NO ports when the channel is ON |
Δron | Difference of ron between channels |
ron(flat) | Difference between the maximum and minimum value of ron in a channel over the specified range of conditions |
INC(OFF) | Leakage current measured at the NC port, with the corresponding channel (NC to COM) in the OFF state under worst-case input and output conditions |
INO(OFF) | Leakage current measured at the NO port, with the corresponding channel (NO to COM) in the OFF state under worst-case input and output conditions |
INC(ON) | Leakage current measured at the NC port, with the corresponding channel (NC to COM) in the ON state and the output (COM) being open |
INO(ON) | Leakage current measured at the NO port, with the corresponding channel (NO to COM) in the ON state and the output (COM) being open |
ICOM(ON) | Leakage current measured at the COM port, with the corresponding channel (NO to COM or NC to COM) in the ON state and the output (NC or NO) being open |
VIH | Minimum input voltage for logic high for the control input (IN) |
VIL | Minimum input voltage for logic low for the control input (IN) |
VIN | Voltage at IN |
IIH, IIL | Leakage current measured at IN |
tON | Turnon time for the switch. Measure this parameter under the specified range of conditions and by the propagation delay between the digital control (IN) signal and analog output (COM/NC/NO) signal when the switch is turning ON. |
tOFF | Turnoff time for the switch. Measure this parameter under the specified range of conditions and by the propagation delay between the digital control (IN) signal and analog output (COM/NC/NO) signal when the switch is turning OFF. |
tBBM | Break-before-make time. Measure this parameter under the specified range of conditions and by the propagation delay between the output of two adjacent analog channels (NC and NO) when the control signal changes state. |
QC | Charge injection is a measurement of unwanted signal coupling from the control (IN) input to the analog (NC, NO, or COM) output. This measure is in coulombs (C) and is the total charge induced due to switching of the control input. Charge injection, QC = CL× ΔVO, CL is the load capacitance and ΔVO is the change in analog output voltage. |
CNC(OFF) | Capacitance at the NC port when the corresponding channel (NC to COM) is OFF |
CNO(OFF) | Capacitance at the NO port when the corresponding channel (NC to COM) is OFF |
CNC(ON) | Capacitance at the NC port when the corresponding channel (NC to COM) is ON |
CNO(ON) | Capacitance at the NO port when the corresponding channel (NC to COM) is ON |
CCOM(ON) | Capacitance at the COM port when the corresponding channel (COM to NC or COM to NO) is ON |
CIN | Capacitance of IN |
OISO | OFF isolation of the switch is a measurement of OFF-state switch impedance. This measure is in dB at a specific frequency, with the corresponding channel (NC to COM or NO to COM) in the OFF state. OFF isolation, OISO = 20 LOG (VNC/VCOM) dB, VCOM is the input and VNC is the output. |
XTALK | Crosstalk is a measurement of unwanted signal coupling from an ON channel to an OFF channel (NC to NO or NO to NC). This measure is at a specific frequency and in dB. Crosstalk, XTALK = 20 log (VNC1/VNO1), VNO1 is the input and VNC1 is the output. |
BW | Bandwidth of the switch. This is the frequency where the gain of an ON channel is –3 dB below the dc gain. Gain is measured from the equation, 20 log (VNC/VCOM) dB, where VNC is the output and VCOM is the input. |
I+ | Static power-supply current with the control (IN) pin at V+ or GND |
ΔI+ | This is the increase in I+ for each control (IN) input that is at the specified voltage, rather than at V+ or GND. |