SLLSFL2A April 2022 – May 2024 TUSB1142
PRODUCTION DATA
Linearity VOD defines the linearity range of the TUSB1142. When TUSB1142 is in linear VOD mode, the output VOD is a linear function of the input VID. For example, if the signal at TUSB1142's input (VID) is at 600 mVpp then the TUSB1142's output VOD will be around 600 mVpp. Linearity VOD mode is the default operation of the TUSB1142. Linear VOD mode is supported on SSRX and CTX1/2 transmitters.
The TUSB1142 provides four different linearity VOD settings. All four settings are available in I2C mode through register control. In pin-strap mode, the linearity is fixed at the highest setting.