SLLSEW6C November 2016 – June 2018 TUSB422
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
A Dual-Role port functions as both a DFP and a UFP. The TUSB422 supports DRP either autonomously or manually. In autonomous DRP mode, the TUSB422 state machine toggles between UFP (Rd) and DFP (Rp) on both its CC pins. Autonomous DRP is enabled by programming Role Control register to 0x4A and writing Looking4Connection command to the Command register. Manual mode is under complete control of external processor. External processor must toggle between writing 0x0A and 0x05 to Role Control register at interval defined by Type-C specification summarized in Table 2.
PARAMETER | MIN | MAX | DESCRIPTION |
---|---|---|---|
tDRP | 50 ms | 100 ms | The period a DRP shall complete a Source (Rp) to Sink (Rd) and back advertisement |
dcSRC.DRP | 30% | 70% | The percent of time that DRP shall advertise Source (Rp) during tDRP . |
The following steps are for initialization of the TUSB422 for DRP operation.
The TUSB422 autonomously toggles between Rd and Rp according to the setting of the CC General Control register. If a value other than default value is desired, then CC General control should be programmed to desired value before performing Step 6.