SLLSFZ6 November 2024 TUSB5461-Q1
ADVANCE INFORMATION
Linearity VOD defines the linearity range of the TUSB5461-Q1. When the TUSB5461-Q1 is in linear VOD mode, the output VOD is a linear function of the input VID. For example, if the signal at TUSB5461-Q1 input (VID) is at 600mVpp then the TUSB5461-Q1 output VOD is approximately 600mVpp. The linear VOD mode is the only mode available for the downstream paths (DisplayPort and USB). The upstream path (USB only) supports both linear and limited VOD. Linearity VOD mode is the default operation of the TUSB5461-Q1. The TUSB5461-Q1 provides four different linearity VOD settings. All four settings are available in I2C mode through register control.