SLLSF93 June 2019 TUSB8042A
PRODUCTION DATA.
When the SMBus interface mode is enabled, the TUSB8042A supports read block and write block protocols as a slave-only SMBus device.
The TUSB8042A slave address is 1000 1xyz, where:
For details on SMBus requirements, refer to the System Management Bus Specification.
NOTE
If the TUSB8042A is addressed by a host using an unsupported protocol it does not respond. The TUSB8042A waits indefinitely for configuration by the SMBus host and doesnot connect on the upstream port until the SMBus host indicates configuration is complete by clearing the CFG_ACTIVE bit.