To begin the design process, determine the following:
- Input voltage range
- Use the supply voltage of the device that is driving the TXS0102V device to determine the input voltage range.
For a valid logic high the value must exceed the VIH of the input port.
For a valid logic low the value must be less than the VIL of the input
port.
- Output voltage range
- Use the supply voltage of the device that the TXS0102V
device is driving to determine the output voltage range.
- The TXS0102V device has 10kΩ internal pullup
resistors. External pullup resistors can be added to reduce the total RC
of a signal trace if necessary.
- An external pull down resistor decreases the output VOH and VOL. Use Equation 1 to calculate the VOH as a result of an
external pull down resistor.
- Where:
- VCCx is the supply voltage on either VCCA or
VCCB
- RPD is the value of the external pull down resistor