SCES861F June 2015 – November 2024 TXS0108E-Q1
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The TXS0108E-Q1 has an OE pin input that is used to disable the device by setting the OE pin low, which places all I/Os in the Hi-Z state. The disable time (tdis) indicates the delay between the time when the OE pin goes low and when the outputs actually get disabled (Hi-Z). The enable time (ten) indicates the amount of time the design must allow for the one-shot circuitry to become operational after the OE pin goes high.