SLUSAG0A March 2011 – March 2016 UC1707-SP
PRODUCTION DATA.
UC1707-SP was designed specifically as a power MOSFET driver for switching-mode power supply applications. It is capable of providing fast transitions and high-peak current required by power MOSFETs. One of the most important factors while developing the UC1707-SP was to isolate the high speed switching noise from the low level analog signals at the PWM. Separate supply and return paths at the driver signal inputs and power outputs further enhance noise immunity.
The function of the circuitry is to be able to provide a shutdown of the device. This is defined as functionality that will drive both outputs to the low state. There are three different inputs that govern this shutdown capability.
To use the Shutdown Pin with the Latch Disable functional it is necessary to use either a diode in series with the Shutdown signal or to use an open collector pullup so that the Shutdown pin is not pulled low. This configuration will allow the Latch Disable function to work with the Shutdown pin.
ANALOG STOP LOGIC | SHUTDOWN | LATCH DISABLE | PREVIOUS STATE OF OUTPUT | OUTPUT |
---|---|---|---|---|
X | 0 | X | X | Follows Input Logic |
X | 1 | X | X | Low (Shutdown) |
1 | Open | X | X | Low (Shutdown) |
0 | Open | 0 | Shutdown | Latched Shutdown(1) |
0 | Open | 0 | Normal | Follows Input Logic |
0 | Open | 1 | X | Follows Input Logic |