SLUSCU6C August 2017 – January 2020 UCC256301
PRODUCTION DATA.
The BLK pin is used to sense the LLC DC input voltage (bulk voltage) level. The comparators on BLK pin set the following thresholds:
BLKOV signal is generated by one comparator with two thresholds selected by a MUX. This is to create necessary hysteresis for the BLKOV fault. The BLKSns signal is buffered and sent to burst mode threshold generation block to implement the adaptive burst mode threshold.
Figure 36 shows the block diagram of the BLK pin.