SLUSEX3C April 2023 – July 2024 UCC27301A-Q1
PRODMIX
Refer to the PDF data sheet for device specific package drawings
Generally, the switching speed of the power switch during turnon and turnoff should be as fast as possible in order to minimize switching power losses. The gate driver device must be able to provide the required peak current for achieving the targeted switching speeds with the targeted power MOSFET. The system requirement for the switching speed is typically described in terms of the slew rate of the drain-to-source voltage of the power MOSFET (such as dVDS/dt). For example, the system requirement might state that a SPP20N60C3 power MOSFET must be turned-on with a dVDS/dt of 20V/ns or higher with a DC bus voltage of 400V in a continuous-conduction-mode (CCM) boost PFC-converter application. This type of application is an inductive hard-switching application and reducing switching power losses is critical. This requirement means that the entire drain-to-source voltage swing during power MOSFET turnon event (from 400V in the OFF state to VDS(on) in on state) must be completed in approximately 20ns or less. When the drain-to-source voltage swing occurs, the Miller charge of the power MOSFET (QGD parameter in the SPP20N60C3 data sheet is 33nC typical) is supplied by the peak current of gate driver. According to power MOSFET inductive switching mechanism, the gate-to-source voltage of the power MOSFET at this time is the Miller plateau voltage, which is typically a few volts higher than the threshold voltage of the power MOSFET, VGS(TH).
To achieve the targeted dVDS/dt, the
gate driver must be capable of providing the QGD charge in 20ns or less.
In other words a peak current of 1.65A (= 33nC/20ns) or higher must be provided by
the gate driver. The UCC27301A-Q1 gate driver is capable of providing 3.7A peak
sourcing current which clearly exceeds the design requirement and has the capability
to meet the switching speed needed. The overdrive capability provides an extra
margin against part-to-part variations in the QGD parameter of the power
MOSFET along with additional flexibility to insert external gate resistors and fine
tune the switching speed for efficiency versus EMI optimizations. However, in
practical designs the parasitic trace inductance in the gate drive circuit of the
PCB will have a definitive role to play on the power MOSFET switching speed. The
effect of this trace inductance is to limit the dI/dt of the output current pulse of
the gate driver. In order to illustrate this, consider output current pulse waveform
from the gate driver to be approximated to a triangular profile, where the area
under the triangle
(½ × IPEAK × time)
would equal the total gate charge of the power MOSFET (QG parameter in
SPP20N60C3 power MOSFET datasheet = 87nC typical). If the parasitic trace inductance
limits the dI/dt then a situation may occur in which the full peak current
capability of the gate driver is not fully achieved in the time required to deliver
the QG required for the power MOSFET switching. In other words the time
parameter in the equation would dominate and the IPEAK value of the
current pulse would be much less than the true peak current capability of the
device, while the required QG is still delivered. Because of this, the
desired switching speed may not be realized, even when theoretical calculations
indicate the gate driver is capable of achieving the targeted switching speed. Thus,
placing the gate driver device very close to the power MOSFET and designing a tight
gate drive-loop with minimal PCB trace inductance is important to realize the full
peak-current capability of the gate driver.