SLUSEY3 July 2024 UCC27311A
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
Generally, the switching speed of the power switch during turnon and turnoff should be as fast as possible in order to minimize switching power losses. The gate driver device must be able to provide the required peak current for achieving the targeted switching speeds with the targeted power MOSFET. The system requirement for the switching speed is typically described in terms of the slew rate of the drain-to-source voltage of the power MOSFET (such as dVDS/dt). For example, the system requirement might state that a SPP20N60C3 power MOSFET must be turned-on with a dVDS/dt of 20V/ns or higher with a DC bus voltage of 400V in a continuous-conduction-mode (CCM) boost PFC-converter application. This type of application is an inductive hard-switching application and reducing switching power losses is critical. This requirement means that the entire drain-to-source voltage swing during power MOSFET turnon event (from 400V in the OFF state to VDS(on) in on state) must be completed in approximately 20ns or less. When the drain-to-source voltage swing occurs, the Miller charge of the power MOSFET (QGD parameter in the SPP20N60C3 data sheet is 33nC typical) is supplied by the peak current of gate driver. According to power MOSFET inductive switching mechanism, the gate-to-source voltage of the power MOSFET at this time is the Miller plateau voltage, which is typically a few volts higher than the threshold voltage of the power MOSFET, VGS(TH).
To achieve the targeted dVDS/dt, the
gate driver must be capable of providing the QGD charge in 20ns or less.
In other words a peak current of 1.65A (= 33nC/20ns) or higher must be provided by
the gate driver. The UCC27311A gate driver is capable
of providing 3.7A peak sourcing current which clearly exceeds the design requirement
and has the capability to meet the switching speed needed. The overdrive capability
provides an extra margin against part-to-part variations in the QGD
parameter of the power MOSFET along with additional flexibility to insert external
gate resistors and fine tune the switching speed for efficiency versus EMI
optimizations. However, in practical designs the parasitic trace inductance in the
gate drive circuit of the PCB will have a definitive role to play on the power
MOSFET switching speed. The effect of this trace inductance is to limit the dI/dt of
the output current pulse of the gate driver. In order to illustrate this, consider
output current pulse waveform from the gate driver to be approximated to a
triangular profile, where the area under the triangle
(½ × IPEAK × time) would equal the total gate charge of the power MOSFET
(QG parameter in SPP20N60C3 power MOSFET datasheet = 87nC typical).
If the parasitic trace inductance limits the dI/dt then a situation may occur in
which the full peak current capability of the gate driver is not fully achieved in
the time required to deliver the QG required for the power MOSFET
switching. In other words the time parameter in the equation would dominate and the
IPEAK value of the current pulse would be much less than the true
peak current capability of the device, while the required QG is still
delivered. Because of this, the desired switching speed may not be realized, even
when theoretical calculations indicate the gate driver is capable of achieving the
targeted switching speed. Thus, placing the gate driver device very close to the
power MOSFET and designing a tight gate drive-loop with minimal PCB trace inductance
is important to realize the full peak-current capability of the gate driver.