SLUSD05B October 2017 – August 2018 UCC27710
PRODUCTION DATA.
The UCC27710 device has a minimum turn-on, turn-off pulse transfer function to the output pin from the input pin. This function ensures UCC27710 is in the correct state when the input signal is very narrow. The function is summarized in Figure 36 and Figure 37. The tON which is 40 ns typical is shown in Figure 36 and tOFF which is 40 ns typical is shown in Figure 37