The UCC28019A 8-pin active Power Factor Correction (PFC) controller uses the boost topology operating in Continuous Conduction Mode (CCM). The controller is suitable for systems in the 100 W to >2 kW range over a wide-range universal ac line input. Start-up current during undervoltage lockout is less than 200 μA. The user can control low power standby mode by pulling the VSENSE pin below 0.77 V.
Low-distortion wave shaping of the input current using average current mode control is achieved without input line sensing, reducing the external component count. Simple external networks allow for flexible compensation of the current and voltage control loops. The switching frequency is internally fixed and trimmed to better than ±5% accuracy at 25°C. Fast 1.5-A peak gate current drives the external switch.
Numerous system-level protection features include peak current limit, soft over-current, open-loop detection, input brown-out, and output over/undervoltage. Soft-start limits boost current during start-up. A trimmed internal reference provides accurate protection thresholds and a regulation set-point. An internal clamp limits the gate drive voltage to 12.5 V.
PART NUMBER | PACKAGE | BODY SIZE (NOM) |
---|---|---|
UCC28019A | SOIC (8) | 3.91 mm × 4.9 mm |
PDIP (8) | 6.35 mm × 9.81 mm |
Changes from C Revision (August 2015) to D Revision
Changes from B Revision (April 2009) to C Revision
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
SOIC, PDIP | |||
GND | 1 | — | Ground: device ground reference. |
ICOMP | 2 | O | Current loop compensation: Transconductance current amplifier output. A capacitor connected to GND provides compensation and averaging of the current sense signal in the current control loop. The controller is disabled if the voltage on ICOMP is less than 0.6 V. |
ISENSE | 3 | I | Inductor current sense: Input for the voltage across the external current sense resistor, which represents the instantaneous current through the PFC boost inductor. This voltage is averaged by the current amplifier to eliminate the effects of ripple and noise. Soft Over Current (SOC) limits the average inductor current. Cycle-by-cycle Peak Current Limit (PCL) immediately shuts off the GATE drive if the peak-limit voltage is exceeded. An internal 1.5-μA current source pulls ISENSE above 0.1 V to shut down PFC operation if this pin becomes open-circuited. Use a 220-Ω resistor between this pin and the current sense resistor to limit inrush-surge currents into this pin. |
VINS | 4 | I | Input ac voltage sense: A filtered resistor-divider network connects from this pin to the rectified-mains node. Input Brown-Out Protection (IBOP) detects when the system ac-input voltage is above a user-defined normal operating level, or below a user-defined “brown-out” level. At startup the controller is disabled until the VINS voltage exceeds a threshold of 1.5 V, initiating a soft start. The controller is also disabled if VINS drops below the brown-out threshold of 0.8 V. Operation will not resume until both VINS and VSENSE voltages exceed their enable thresholds, initiating another soft start. |
VCOMP | 5 | O | Voltage loop compensation: Transconductance voltage error amplifier output. A resistor-capacitor network connected from this pin to GND provides compensation. VCOMP is held at GND until VCC, VINS, and VSENSE all exceed their threshold voltages. Once these conditions are satisfied, VCOMP is charged until the VSENSE voltage reaches 99% of its nominal regulation level. When Enhanced Dynamic Response (EDR) is engaged, a higher transconductance is applied to VCOMP to reduce the charge time for faster transient response. Soft Start is programmed by the capacitance on this pin. The EDR higher transconductance is inhibited during Soft Start. |
VSENSE | 6 | I | Output voltage sense: An external resistor-divider network connected from this pin to the PFC output voltage provides feedback sensing for regulation to the internal 5-V reference voltage. A small capacitor from this pin to GND filters high-frequency noise. Standby mode disables the controller and discharges VCOMP when the voltage at VSENSE drops below the enable threshold of 0.8 V. An internal 100-nA current source pulls VSENSE to GND for Open-Loop Protection (OLP), including pin disconnection. Output Over-Voltage Protection (OVP) disables the GATE output when VSENSE exceeds 105% of the reference voltage. Enhanced Dynamic Response (EDR) rapidly returns the output voltage to its normal regulation level when a system line or load step causes VSENSE to fall below 95% of the reference voltage. |
VCC | 7 | Device supply: External bias supply input. Under-Voltage Lockout (UVLO) disables the controller until VCC exceeds a turn-on threshold of 10.5 V. Operation continues until VCC falls below the turn-off (UVLO) threshold of 9.5 V. A ceramic by-pass capacitor of 0.1 μF minimum value should be connected from VCC to GND as close to the device as possible for high frequency filtering of the VCC voltage. | |
GATE | 8 | O | Gate drive: Integrated push-pull gate driver for one or more external power MOSFETs. Typical 2.0-A sink and 1.5-A source capability. Output voltage is typically clamped at 12.5 V. |
MIN | MAX | UNIT | ||
---|---|---|---|---|
Input voltage range | VCC, GATE | –0.3 | 22 | V |
VINS, VSENSE, | –0.3 | 7 | V | |
VCOMP, ICOMP(2) | –0.3 | 7.5 | V | |
ISENSE | –24 | 7 | V | |
Input current range | VSENSE, ISENSE | –1 | 1 | mA |
Lead temperature, TSOL | Soldering, 10s | 300 | °C | |
Junction temperature, TJ | Operating | –55 | 150 | °C |
Storage | –65 | 150 | °C |
VALUE | UNIT | |||
---|---|---|---|---|
V(ESD) | Electrostatic discharge | Human-body model (HBM), per ANSI/ESDA/JEDEC JS-001(1) | ±2000 | V |
Charged-device model (CDM), per JEDEC specification JESD22-C101(2) | ±500 | V |
MIN | MAX | UNIT | |
---|---|---|---|
VCC input voltage from a low-impedance source | VCCOFF + 1 V | 21 | V |
Operating junction temperature, TJ | -40 | 125 | °C |
THERMAL METRIC(1) | UCC28019A | UNIT | ||
---|---|---|---|---|
P (PDIP) | D (SOIC) | |||
8 PINS | 8 PINS | |||
RθJA | Junction-to-ambient thermal resistance | 52.8 | 113.0 | °C/W |
RθJC(top) | Junction-to-case (top) thermal resistance | 42.3 | 61.5 | °C/W |
RθJB | Junction-to-board thermal resistance | 30.0 | 53.2 | °C/W |
ψJT | Junction-to-top characterization parameter | 19.5 | 15.9 | °C/W |
ψJB | Junction-to-board characterization parameter | 29.9 | 52.7 | °C/W |
PARAMETER | TEST CONDITION | MIN | TYP | MAX | UNIT | |
---|---|---|---|---|---|---|
VCC Bias Supply | ||||||
ICCPRESTART | ICC pre-start current | VCC = VCCON – 0.1 V | 25 | 100 | 200 | μA |
ICCSTBY | ICC standby current | VSENSE = 0.5 V | 1 | 2.2 | 2.9 | mA |
ICCON_load | ICC operating current | VSENSE = 4.5 V, CGATE = 4.7 nF | 4 | 7.5 | 10 | mA |
Under Voltage Lockout (UVLO) | ||||||
VCCON | VCC turn on threshold | 10 | 10.5 | 11 | V | |
VCCOFF | VCC turn off threshold | 9 | 9.5 | 10 | V | |
UVLO hysteresis | 0.8 | 1 | 1.2 | V | ||
Oscillator | ||||||
fSW | Switching frequency | TA = 25°C | 61.7 | 65 | 68.3 | kHz |
-25°C ≤ TA ≤ 125°C | 59 | 65 | 71 | kHz | ||
-40°C ≤ TA ≤ 125°C | 57 | 71 | kHz | |||
PWM | ||||||
DMIN | Minimum duty cycle | VCOMP = 0 V, VSENSE = 5 V, ICOMP = 6.4 V |
0% | |||
DMAX | Maximum duty cycle | VSENSE = 4.95 V | 94% | 98% | 99.3% | |
tOFF(min) | Minimum off time | VSENSE = 3 V, ICOMP = 1 V | 100 | 250 | 600 | ns |
System Protection | ||||||
VSOC | ISENSE threshold, Soft Over Current (SOC) | -0.66 | -0.73 | -0.79 | V | |
VPCL | ISENSE threshold, Peak Current Limit (PCL) | -1 | -1.08 | -1.15 | V | |
IISOP | ISENSE bias current, ISENSE Open-Pin Protection (ISOP) | ISENSE = 0 V | -2.1 | -4.0 | μA | |
VISOP | ISENSE threshold, ISENSE Open-Pin Protection (ISOP) | ISENSE = open pin | 0.082 | V | ||
VOLP | VSENSE threshold, Open Loop Protection (OLP) | ICOMP = 1 V, ISENSE = -0.1 V, VCOMP = 1 V |
0.77 | 0.82 | 0.86 | V |
Open Loop Protection (OLP) Internal pull-down current | VSENSE = 0.5 V | 100 | 250 | nA | ||
VUVD | VSENSE threshold, output Under-Voltage Detection (UVD)(1) | 4.63 | 4.75 | 4.87 | V | |
VOVP | VSENSE threshold, output Over-Voltage Protection (OVP) | ISENSE = -0.1 V | 5.12 | 5.25 | 5.38 | V |
VINSBROWNOUT_th | Input Brown-Out Detection (IBOP) high-to-low threshold |
0.76 | 0.82 | 0.88 | V | |
VINSENABLE_th | Input Brown-Out Detection (IBOP) low-to-high threshold |
1.4 | 1.5 | 1.6 | V | |
IVINS_0V | VINS bias current | VINS = 0 V | 0 | ±0.1 | μA | |
ICOMP threshold, external overload protection | 0.6 | V | ||||
Current Loop | ||||||
gmi | Transconductance gain | TA = 25°C | 0.75 | 0.95 | 1.15 | mS |
Output linear range(1) | ±50 | μA | ||||
ICOMP voltage during OLP | VSENSE = 0.5 V | 3.7 | 4 | 4.3 | V | |
Voltage Loop | ||||||
VREF | Reference voltage | -40°C ≤ TA ≤ 125°C | 4.9 | 5 | 5.1 | V |
gmv | Transconductance gain without EDR | -31.5 | -42 | -52.5 | μS | |
gmv-EDR | Transconductance gain under EDR | VSENSE = 4.65 V | -440 | μS | ||
Maximum sink current under normal operation | VSENSE = 6 V, VCOMP = 4 V | 21 | 30 | 38 | μA | |
Source current under soft start | VSENSE = 4 V, VCOMP = 2.5 V | -21 | -30 | -38 | μA | |
Maximum source current under EDR operation | VSENSE = 4 V, VCOMP = 2.5 V | -300 | μA | |||
VSENSE = 4 V, VCOMP = 4 V | -170 | μA | ||||
Enhanced dynamic response VSENSE low threshold, falling(1) | 4.63 | 4.75 | 4.87 | V | ||
VSENSE input bias current | VSENSE = 5 V | 20 | 100 | 250 | nA | |
VCOMP voltage during OLP | VSENSE = 0.5 V, IVCOMP = 0.5 mA | 0 | 0.2 | 0.4 | V | |
VCOMP rapid discharge current | VCOMP = 3 V, VCC = 0 V | 0.77 | mA | |||
VPRECHARGE | VCOMP precharge voltage | IVCOMP = -100 μA, VSENSE = 5 V | 1.76 | V | ||
IPRECHARGE | VCOMP precharge current | VCOMP = 1.0 V | -1 | mA | ||
VSENSE threshold, end of soft start | Initial start up | 4.95 | V | |||
GATE Driver | ||||||
GATE current, peak, sinking(1) | CGATE = 4.7 nF | 2 | A | |||
GATE current, peak, sourcing(1) | CGATE = 4.7 nF | -1.5 | A | |||
GATE rise time | CGATE = 4.7 nF, GATE = 2 V to 8 V | 8 | 40 | 60 | ns | |
GATE fall time | CGATE = 4.7 nF, GATE = 8 V to 2 V | 8 | 25 | 40 | ns | |
GATE low voltage, no load | I GATE = 0 A | 0 | 0.05 | V | ||
GATE low voltage, sinking | I GATE = 20 mA | 0.3 | 0.8 | V | ||
GATE low voltage, sourcing | I GATE = -20 mA | -0.3 | -0.8 | V | ||
GATE low voltage, sinking, device OFF | VCC = 5 V, IGATE = 5 mA | 0.2 | 0.75 | 1.2 | V | |
VCC = 5 V, IGATE = 20 mA | 0.2 | 0.9 | 1.5 | V | ||
GATE high voltage | VCC = 20 V, CGATE = 4.7 nF | 11.0 | 12.5 | 14.0 | V | |
VCC = 11 V, CGATE = 4.7 nF | 9.5 | 10.5 | 11.0 | V | ||
VCC = VCCOFF + 0.2 V, CGATE = 4.7 nF | 8.0 | 9.4 | 10.2 | V |
The UCC28019A is a switch-mode controller used in boost converters for power factor correction operating at a fixed frequency in continuous conduction mode. The UCC28019A requires few external components to operate as an active PFC pre-regulator. Its trimmed oscillator provides a nominal fixed switching frequency of 65 kHz, ensuring that both the fundamental and second harmonic components of the conducted-EMI noise spectrum are below the EN55022 conducted-band 150 kHz measurement limit.
Its tightly-trimmed internal 5-V reference voltage provides for accurate output voltage regulation over the typical world-wide 85-265VAC mains input range from zero to full output load.
Regulation is accomplished in two loops. The inner current loop shapes the average input current to match the sinusoidal input voltage under continuous inductor current conditions. Under light load conditions, depending on the boost inductor value, the inductor current may go discontinuous but still meet Class-D requirements of EN61000-3-2 despite the higher harmonics. The outer voltage loop regulates the PFC output voltage by generating a voltage on VCOMP (dependent upon the line and load conditions) which determines the internal gain parameters for maintaining a low-distortion steady-state input current wave-shape.
Soft Start controls the rate of rise of VCOMP in order to obtain a linear control of the increasing duty cycle as a function of time. VCOMP, the output of the voltage loop transconductance amplifier, is pulled low during UVLO, IBOP, and OLP (Open-Loop Protection)/STANDBY. Once the fault condition is released, an initial pre-charge source rapidly charges VCOMP to about 1.9 V. After that point, a constant 30 μA of current is sourced into the compensation components causing the voltage on this pin to ramp linearly until the output voltage reaches 85% of its final value. At this point, the sourcing current decreases until the output voltage reaches 99% of its final rated voltage. The Soft-Start time is controlled by the voltage error amplifier compensation capacitor values selected, and is user programmable based on desired loop crossover frequency. Once the output voltage exceeds 99% of rated voltage, the pre-charge source is discountinued and EDR is no longer inhibited.
System-level protection features help keep the converter within safe operating limits.
During startup, Under-Voltage Lockout (UVLO) keeps the device in the off state until VCC rises above the 10.5-V enable threshold, VCCON. With a typical 1 V of hysteresis on UVLO to increase noise immunity, the device turns off when VCC drops to the 9.5-V disable threshold, VCCOFF.
If, during a brief ac-line dropout, the VCC voltage falls below the level necessary to bias the internal FAULT circuitry, the UVLO condition enables a special rapid discharge circuit which continues to discharge the VCOMP capacitors through a low impedance despite a complete lack of VCC. This helps to avoid an excessive current surge should the ac-line return while there is still substantial voltage stored on the VCOMP capacitors. Typically, these capacitors can be discharged to less than 1.2 V within 150 ms of loss of VCC.
The sensed line-voltage input, VINS, provides a means for the designer to set the desired mains RMS voltage level at which the PFC pre-regulator should start-up, VACturnon, as well as the desired mains RMS level at which it should shut down, VACturnoff. This prevents unwanted sustained system operation at or below a brown-out voltage, where excessive line current could overheat components. In addition, because VCC bias is not derived directly from the line voltage, IBOP protects the circuit from low line conditions that may not trigger the VCC UVLO turn-off.
Input line voltage is sensed directly from the rectified ac mains voltage through a resistor-divider filter network providing a scaled and filtered value at the VINS input. IBOP will put the device into standby mode when VINS falls (high to low) below 0.8 V, VINSBROWNOUT_th. The device comes out of standby when VINS rises (low to high) above 1.5 V, VINSENABLE_th. Bias current sourced from VINS, IVINS_0V, is less than 0.1 μA. With a bias current this low, there is little concern for any set-point error caused by this current flowing through the sensing network. The highest praticable value resistance for this network should be chosen to minimize power dissipation, especially in applications requiring low standby power. Be aware that higher resistance values are more susceptible to noise pickup, but low-noise PCB layout techniques can help mitigate this. Also, depending on the resistor type used and its voltage rating, RVINS1 should be implemented with multiple resistors in series to reduce voltage stresses.
First, select RVINS1 based on choosing the highest reasonable resistance value available for typical applications.
Then select RVINS2 based on this value:
Power dissipated in the resistor network is:
The filter capacitor, CVINS, has two functions. First, to attenuate the voltage ripple to levels between the enable and brown-out threshold to prevent ripple on VINS from falsely triggering IBOP when the converter is operating at low line. Second, CVINS delays the brown-out protection operation for a desired number of line-half-cycle periods while still having a good response to an actual brown-out event.
The capacitor is chosen so that it will discharge to the VINSBROWNOUT_th level after a delay of N number of line ½-cycles to accommodate ac-line dropout ride-through requirements.
Where,
and VACmin is the lowest normal operating rms input voltage.
VOUT(OVP) is the output voltage exceeding 5% of the rated value, causing VSENSE to exceed a 5.25-V threshold (5-V reference voltage + 5%), VOVP. The normal control loop is bypassed and the GATE output is disabled until VSENSE falls below 5.25 V. VOUT(OVP) is 420 V in a system with a 400-V rated output, for example.
If the output voltage feedback components were to fail and disconnect (open loop) the signal from the VSENSE input, then it is likely that the voltage error amp would increase the GATE output to maximum duty cycle. To prevent this, an internal pull-down forces VSENSE low. If the output voltage falls below 16% of its rated voltage, causing VSENSE to fall below 0.8 V, the device is put in standby, a state where the PWM switching is halted and the device is still on but draws standby current below 2.9 mA. This shutdown feature also gives the designer the option of pulling VSENSE low with an external switch.
If the current feedback components were to fail and disconnect (open loop) the signal to the ISENSE input, then it is likely that the PWM stage would increase the GATE output to maximum duty cycle. To prevent this, an internal pull-up source drives ISENSE above 0.1 V so that a detector forces a state where the PWM switching is halted and the device is still on but draws standby current below 2.9 mA. This shutdown feature avoids continual operation in OVP and severely distorted input current.
During normal operation, small perturbations on the PFC output voltage rarely exceed 5% deviation and the normal voltage control loop gain drives the output back into regulation. For large changes in line or load, if the output voltage drop exceeds -5%, an output under-voltage is detected (UVD) and Enhanced Dynamic Response (EDR) acts to speed up the slow response of the low-bandwidth voltage loop. During EDR, the transconductance of the voltage error amplifier is increased approximately 16 times to speed charging of the voltage-loop compensation capacitors to the level required for regulation. EDR is removed when VSENSE > 4.75 V. The EDR feature is not activated until soft start is completed.
Inductor current is sensed by RISENSE, a low value resistor in the return path of input rectifier. The other side of the resistor is tied to the system ground. The voltage is sensed on the rectifier side of the sense resistor and is always negative. The voltage at ISENSE is buffered by a fixed gain of -1.0 to provide a positive internal signal to the current functions. There are two over-current protection features; Soft Over-Current (SOC) protects against an overload on the output and Peak Current Limit (PCL) protects against inductor saturation.
Soft Over-Current (SOC) limits the input current. SOC is activated when the current sense voltage on ISENSE reaches -0.73 V, affecting the internal VCOMP level, and the control loop is adjusted to reduce the PWM duty cycle.
Peak Current Limit (PCL) operates on a cycle-by-cycle basis. When the current sense voltage on ISENSE reaches -1.08 V, PCL is activated, immediately terminating the active switch cycle. PCL is leading-edge blanked to improve noise immunity against false triggering.
The current sense resistor, RISENSE, is sized using the minimum threshold value of Soft Over Current (SOC), VSOC(min) = 0.66 V. To avoid triggering this threshold during normal operation, resulting in a decreased duty-cycle, the resistor is sized for an overload current of 10% more than the peak inductor current,
Since RISENSE sees the average input current, worst-case power dissipation occurs at input low-line when input current is at its maximum. Power dissipated by the sense resistor is given by:
Peak Current Limit (PCL) protection turns off the output driver when the voltage across the sense resistor reaches the PCL threshold, VPCL. The absolute maximum peak current, IPCL, is given by:
The GATE output is designed with a current-optimized structure to directly drive large values of total MOSFET gate capacitance at high turn-on and turn-off speeds. An internal clamp limits voltage on the MOSFET gate to 12.5 V (typical). When VCC voltage is below the UVLO level, the GATE output is held in the Off state. An external gate drive resistor, RGATE, can be used to limit the rise and fall times and dampen ringing caused by parasitic inductances and capacitances of the gate drive circuit and to reduce EMI. The final value of the resistor depends upon the parasitic elements associated with the layout and other considerations. A 10-kΩ resistor close to the gate of the MOSFET, between the gate and ground, discharges stray gate capacitance and helps protect against inadvertent dv/dt-triggered turn-on.
The overall system current loop consists of the current averaging amplifier stage, the pulse width modulator (PWM) stage, the external boost inductor stage and the external current sensing resistor.
The negative polarity signal from the current sense resistor is buffered and inverted at the ISENSE input. The internal positive signal is then averaged by the current amplifier (gmi), whose output is the ICOMP pin. The voltage on ICOMP is proportional to the average inductor current. An external capacitor to GND is applied to the ICOMP pin for current loop compensation and current ripple filtering. The gain of the averaging amplifier is determined by the internal VCOMP voltage. This gain is non-linear to accommodate the world-wide ac-line voltage range.
ICOMP is connected to 4V internally whenever the device is in a Fault or Standby condition.
The PWM stage compares the ICOMP signal with a periodic ramp to generate a leading-edge-modulated output signal which is High whenever the ramp voltage exceeds the ICOMP voltage. The slope of the ramp is defined by a non-linear function of the internal VCOMP voltage.
The PWM output signal always starts Low at the beginning of the cycle, triggered by the internal clock. The output stays Low for a minimum off-time, tOFF_min, after which the ramp rises linearly to intersect the ICOMP voltage. The ramp-ICOMP intersection determines tOFF, and hence DOFF. Since DOFF = VIN/VOUT by the boost-topology equation, and since VIN is sinusoidal in wave-shape, and since ICOMP is proportional to the inductor current, it follows that the control loop forces the inductor current to follow the input voltage wave-shape to maintain boost regulation. Therefore, the average input current is also sinusoidal in wave-shape.
The output of the PWM comparator stage is conveyed to the GATE drive stage, subject to control by various protection functions incorporated into the device. The GATE output duty-cycle may be as high as 99%, but will always have a minimum off-time tOFF_min. Normal duty-cycle operation can be interrupted directly by OVP and PCL on a cycle-by-cycle basis. UVLO, IBOP and OLP/Standby also terminate the GATE output pulse, and further inhibit output until the SS operation can begin.
The outer control loop of the PFC controller is the voltage loop. This loop consists of the PFC output sensing stage, the voltage error amplifier stage, and the non-linear gain generation.
A resistor-divider network from the PFC output voltage to GND forms the sensing block for the voltage control loop. The resistor ratio is determined by the desired output voltage and the internal 5-V regulation reference voltage.
Like the VINS input, the very low bias current at the VSENSE input allows the choice of the highest practicable resistor values for lowest power dissipation and standby current. A small capacitor from VSENSE to GND serves to filter the signal in a high-noise environment. This filter time constant should generally be less than 100 μs.
The transconductance error amplifier (gmv) generates an output current proportional to the difference between the voltage feedback signal at VSENSE and the internal 5-V reference. This output current charges or discharges the compensation network capacitors on the VCOMP pin to establish the proper VCOMP voltage for the system operating conditions. Proper selection of the compensation network components leads to a stable PFC pre-regulator over the entire ac-line range and 0-100% load range. The total capacitance also determines the rate-of-rise of the VCOMP voltage at soft start, as discussed earlier.
The amplifier output VCOMP is pulled to GND during any Fault or Standby condition to discharge the compensation capacitors to an initial zero state. Usually, the large capacitor has a series resistor which delays complete discharge for their respective time constant (which may be several hundred milliseconds). If VCC bias voltage is quickly removed after UVLO, the normal discharge transistor on VCOMP loses drive and the large capacitor could be left with substantial voltage on it, negating the benefit of a subsequent soft start. The UCC28019A incorporates a parallel discharge path which operates without VCC bias, to further discharge the compensation network after VCC is removed.
When output voltage perturbations greater than ±5% appear at the VSENSE input, the amplifier moves out of linear operation. On an over-voltage, the OVP function acts directly to shut off the GATE output until VSENSE returns within ±5% of regulation. On an under-voltage, the UVD function invokes EDR which immediately increases the voltage error amplifier transconductance to about 440 μS. This higher gain facilitates faster charging of the compensation capacitors to the new operating level.
The voltage at VCOMP is used to set the current amplifier gain and the PWM ramp slope. This voltage is buffered internally and is then subject to modification by the SOC function, as discussed earlier.
Together the current gain and the PWM slope adjust to the different system operating conditions (set by the ac-line voltage and output load level) as VCOMP changes, to provide a low-distortion, high-power-factor input current wave-shape following that of the input voltage.
This device has no functional modes.