SLUSEW0 December 2023 UCC28750
PRODUCTION DATA
The bulk capacitance can consist of a set of one or more capacitors connected in parallel, often with some inductance between them to suppress differential mode noise. Input EMI filter design is outside the scope of this data sheet and is not discussed.
The mimimum bulk voltage valley, Vbulk,min, is dependent on the total input capacitance value used in the power stage design. The input capacitor is chosen to maintain an acceptable input voltage ripple. The ripple is largest at the minimum input line at the largest output power scenario. Therefore, the input bulk capacitance is based on the a wanted Vbulk,min at the max power.
The input power can be estimated by taking the maximum output power and dividing the result by the estimated efficiency.
Where
For this design, the result from taking the design requirements and the plugging in those values to Equation 6 and Equation 7, a recommended minimum of 110μF for the bulk input capacitance.