SLUSB72D March 2013 – April 2021 UCD3138064
PRODUCTION DATA
VGH | – | This is the V33A threshold where the internal power is declared good. The UCD3138064 comes out of reset when above this threshold. |
VGL | – | This is the V33A threshold where the internal power is declared bad. The device goes into reset when below this threshold. |
Vres | – | This is the V33A threshold where the internal reset signal is no longer valid. Below this threshold the device is in an indeterminate state. |
IReset | – | This is the internal reset signal. When low, the device is held in reset. This is equivalent to holding the reset pin on the IC low. |
TPOR | – | The time delay from when VGH is exceeded to when the device comes out of reset. |
Brown Out | – | This is the V33A voltage threshold at which the device sets the brown out status bit. In addition an interrupt can be triggered if enabled. |