SLVSDD4C September 2016 – March 2020 UCD90160A
PRODUCTION DATA.
Pins 31, 32, 41, and 42 can be used as GPIs or PWM outputs.
If configured as PWM outputs, then limitations apply:
The frequency for PWM3 and PWM4 is derived by dividing down a 15.625-MHz clock. To determine the actual frequency to which these PWMs can be set, must divide 15.625 MHz by any integer between 2 and (224 – 1). The duty cycle resolution will be dependent on the set frequency for PWM3 and PWM4.
The PWM3 or PWM4 duty cycle resolution is dependent on the frequency set for the given PWM. Once the frequency is known the duty cycle resolution can be calculated as Equation 2.
To determine the closest frequency to 1 MHz that PWM3 can be set to calculate as the following:
All frequencies below 238 Hz will have a duty cycle resolution of 0.0015%.