SLVSCW0 February 2015 UCD90240
PRODUCTION DATA.
UCD90240 is in a 157-pin BGA package. If UCD90240 is mounted on the top layer, decoupling capacitors can be placed on the bottom layer to make room for top-layer trace routing. The layout example below adopts such a strategy. Figure 35 shows bottom-layer component placement from top-view. In addition to Figure 35, note that: