SLUSDC1 September 2018 UCD90320U
PRODUCTION DATA.
The UCD90320U provides fault log, device reset counter, and peak readings for each rail. To reduce stress on the EEPROM memory, a 30-second timer is started if a measured value exceeds the previously logged value. Only the highest value from the 30-second interval is written from RAM to EEPROM.
Faults are stored in EEPROM memory and are accessible over PMBus. Each logged fault includes the following information:
The total number of device resets is also stored to EEPROM memory. The value can be reset using PMBus.
The run time clock value is logged into EEPROM when a power down is detected. This allows UCD90320U to preserve the run-time clock value through resets or power cycles.
It is also possible to update and calibrate the UCD90320U internal run-time clock via a PMBus host. For example, a host processor with a real-time clock could periodically update the UCD90320U run-time clock to a value that corresponds to the actual date and time. The host must translate the UCD90320U timer value back into appropriate units, based on the usage scenario chosen. See the REAL_TIME_CLOCK command in the UCD90320U Sequencer and System Health Controller PMBus Command Reference for more details.