SLUSDC1 September 2018 UCD90320U
PRODUCTION DATA.
Up to 32 of the 84 GPIO pins of the UCD90320U device can be configured as GPI. The GPI configuration window is under the Pin Assignment tab. Figure 11 shows an example.
The polarity of GPI pins can be configured to be either active high or active low. Each GPI can be used as a source of sequence dependency. (See also the Rail Sequence Configuration section). The GPI pins can be also used for cascading function. (See also the Cascading Multiple Devices section). The first defined 3 GPIs regardless of their main purpose are assigned to the pin selected states function. (See also the Pin Selected Rail States Configuration section).
In addition hard configuration functions, four special behaviors can be assigned to each GPI pin using the dropdown window shown in Figure 12:
Events | Description |
---|---|
VOUT_OV_FAULT | Voltage rail is over OV fault threshold |
VOUT_OV_WARNING | Voltage rail is over OV warning threshold |
VOUT_UV_FAULT | Voltage rail is under UV fault threshold |
VOUT_UV_WARNING | Voltage rail is under UV warning threshold |
TON_MAX | Voltage rail fails to reach power good threshold in predefined period. |
TOFF_MAX Warning | Voltage rail fails to reach power not good threshold in predefined period |
IOUT_OC_FAULT | Current rail is over OC fault threshold |
IOUT_OC_WARNING | Current rail is under OC warning threshold |
IOUT_UC | Current rail is under UC fault threshold |
OT_FAULT | Temperature rail is over OT fault threshold |
OT_WARNING | Temperature rail is over OT warning threshold |
All GPI de-asserted | No logging and fault response, but the function of the GPI is not ignored. |
SYSTEM_WATCHDOG_TIMEOUT | System watch timeout |
RESEQUENCE_ERROR | Rail fails to resequence |
SEQ_ON_TIMEOUT | Rail fails to meeting sequence on dependency in predefined period |
SEQ_OFF_TIMEOUT | Rail fails to meeting sequence on dependency in predefined period |
SLAVE_FAULT | Rail is shut down due to that its master has fault |
SINGLE_EVENT_UPSET | SEU is detected on the configuration SRAM |