SLRS064B June 2014 – August 2016 ULN2003B
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
ULN2003B will typically be used to drive a high voltage and/or current peripheral from an MCU or logic device that cannot tolerate these conditions. The following design is a common application of ULN2003B, driving inductive loads. This includes motors, solenoids and relays. Figure 23 is a typical block diagram representation of this application.
For this design example, use the parameters listed in Table 1 as the input parameters.
DESIGN PARAMETER (1) | EXAMPLE VALUE |
---|---|
GPIO Voltage | 3.3 V or 5 V |
Coil Supply Voltage | 12 V to 48 V |
Number of Channels | 7 |
Output Current (RCOIL) | 20 mA to 300 mA per channel (See Figure 5) |
Duty Cycle | See Figure 6 to Figure 14 |
When using ULN2003B in a coil driving application, determine the following:
The coil current is determined by the coil voltage (VSUP), coil resistance and output low voltage (VOL or VCE(SAT)).
The output low voltage (VOL) is the same thing as VCE(SAT) and can be determined by, Figure 1, Figure 2, or Figure 4.
The number of coils driven is dependent on the coil current and on-chip power dissipation. The number of coils driven can be determined by Figure 6 or Figure 7.
For a more accurate determination of number of coils possible, use Equation 2 to calculate ULN2003B on-chip power dissipation PD:
where
In order to guarantee reliability of ULN2003B and the system the on-chip power dissipation must be lower that or equal to the maximum allowable power dissipation (PD(MAX)) dictated by Equation 3.
where
TI recommends to limit ULN2003B IC’s die junction temperature to less than 125°C. The IC junction temperature is directly proportional to the on-chip power dissipation.
The following curves were generated with ULN2003B driving an OMRON G5NB relay – Vin = 5.0V; Vsup= 12 V and RCOIL= 2.8 kΩ