SBOS375D October 2006 – October 2024 XTR111
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The XTR111 can be configured in either current or voltage output mode. To use the XTR111 in voltage output mode, the load must be connected directly to the SET pin. The following example shows the use of a switch that can allow for selecting current or voltage output.