This document describes the known exceptions to functional specifications (advisories) to the CC2340R5-Q1SimpleLink™ device.
SimpleLink™ and Texas Instruments™ are trademarks of Texas Instruments.
All trademarks are the property of their respective owners.
Table 1-1 lists all advisories, modules affected, and the applicable silicon revisions.
MODULE | DESCRIPTION | SILICON REVISIONS AFFECTED | |||
---|---|---|---|---|---|
B | |||||
SPI | Advisory SPI_04—Hang scenario with SPI waiting for CPU intervention forever | Yes | |||
ADC | Advisory ADC_08—ADC BUSY bit not cleared in repeat single, sequence and repeat sequence conversion modes. | Yes | |||
ADC | Advisory ADC_09—ADC can have random conversion errors. | Yes | |||
BATMON | Advisory BATMON_01—Incorrect temperature measurement | Yes | |||
CKM | Advisory CLK_01—Bluetooth Low Energy link may not be maintained when using LFOSC only | Yes | |||
I2C | Advisory I2C_02—SDA and SCL open-drain output buffer issue | Yes | |||
GPIO | Advisory GPIO_01—Open-drain configuration can drive a short high pulse | Yes |
To designate the stages in the product development cycle, Texas Instruments™ assigns prefixes to the part numbers of all devices and support tools. Each device has one of three prefixes: X, P, or null (for example, XCC2340R5-Q1). Texas Instruments recommends two of three possible prefix designators for its support tools: TMDX and TMDS. These prefixes represent evolutionary stages of product development from engineering prototypes (X/TMDX) through fully qualified production devices/tools (null/TMDS).
Device development evolutionary flow:
Support tool development evolutionary flow:
X and P devices and TMDX development-support tools are shipped against the following disclaimer:
"Developmental product is intended for internal evaluation purposes."
Production devices and TMDS development-support tools have been characterized fully, and the quality and reliability of the device have been demonstrated fully. TI's standard warranty applies.
Predictions show that prototype devices (X or P) have a greater failure rate than the standard production devices. Texas Instruments recommends that these devices not be used in any production system because their expected end-use failure rate is still undefined. Only qualified production devices are to be used.
This document supports the following device:
Figure 2-1 and Table 2-1 describe package symbolization and the device revision code.
Device Revision Code | Silicon Revision |
---|---|
B | PG2.0 |
Hang scenario with SPI waiting for CPU intervention forever.