The following screen shot shows the top layer of the ADC32RF5x EVM.
- The input signal traces are routed as differential signals on
the top layer avoiding vias. Care is taken to maintain symmetry between positive
and negative input with matched trace length in order to minimize phase
imbalance.
Figure 8-7
shows the layout example for 1x and 2x averaging configuration
Figure 8-8 shows the layout example for 4x averaging configuration
- JESD204B output interface lanes are routed differential and
length matched
- Bypass caps are close to the power pins on the top layer
avoiding vias.