JAJSRW8 November 2023 ADC34RF55
PRODUCTION DATA
The following registers start the power up foreground calibration. The register writes need to be written in the order indicated by Write #.
WRITE # | ADDRESS | DATA | WRITE # | ADDRESS | DATA | WRITE # | ADDRESS | DATA |
---|---|---|---|---|---|---|---|---|
1 | 0x05 | 0x20 | 62 | 0xC9 | 0x06 | 123 | 0xAA | 0x80 |
2 | 0xE7 | 0x01 | 63 | 0x38 | 0x01 | 124 | 0xAC | 0x80 |
3 | 0x174 | 0x02 | 64 | 0x110 | 0x10 | 125 | 0xAD | 0x80 |
4 | 0x178 | 0x00 | 65 | 0x111 | 0x42 | 126 | 0xAD | 0x90 |
5 | 0x17C | 0x22 | 66 | 0x112 | 0xA6 | 127 | 0xAD | 0xA0 |
6 | 0x3C | 0x00 | 67 | 0x112 | 0xD6 | 128 | 0xAD | 0xB0 |
7 | 0xFC | 0x03 | 68 | 0x113 | 0xBB | 129 | 0xAD | 0xC0 |
8 | 0xFD | 0x00 | 69 | 0x113 | 0xDB | 130 | 0xAD | 0xD0 |
9 | 0x154 | 0x1C | 70 | 0x114 | 0xF4 | 131 | 0xAD | 0xE0 |
10 | 0x155 | 0x03 | 71 | 0x114 | 0x64 | 132 | 0xA0 | 0x00 |
11 | 0xFC | 0x03 | 72 | 0x115 | 0x0E | 133 | 0xA2 | 0x00 |
12 | 0xEE | 0x26 | 73 | 0x115 | 0xFE | 134 | 0xA4 | 0x00 |
13 | 0xEF | 0x02 | 74 | 0x116 | 0x0D | 135 | 0xA6 | 0x00 |
14 | 0x18C | 0x88 | 75 | 0x116 | 0xDD | 136 | 0xA8 | 0x00 |
15 | 0xAE | 0xC8 | 76 | 0x117 | 0x0D | 137 | 0xAA | 0x00 |
16 | 0xAF | 0x00 | 77 | 0x117 | 0xDD | 138 | 0xAC | 0x00 |
17 | 0xB0 | 0x4C | 78 | 0x46 | 0x03 | 139 | 0xAD | 0x00 |
18 | 0xB1 | 0x3F | 79 | 0x3D | 0x00 | 140 | 0x9D | 0x45 |
19 | 0x4F | 0x46 | 80 | 0x45 | 0x0A | 141 | 0x9D | 0x05 |
20 | 0x50 | 0x2C | 81 | 0x46 | 0x02 | 142 | 0x20 | 0x00 |
21 | 0x51 | 0x05 | 82 | 0x64 | 0x4A | 143 | 0x04 | 0x00 |
22 | 0x154 | 0x7C | 83 | 0x65 | 0x05 | 144 | 0x05 | 0x20 |
23 | 0x158 | 0x7C | 84 | 0x68 | 0x28 | 145 | 0xFE | 0x00 |
24 | 0x159 | 0x6F | 85 | 0x69 | 0x5E | 146 | 0xFF | 0x00 |
25 | 0x15C | 0x7C | 86 | 0x6A | 0x3D | 147 | 0x89 | 0x00 |
26 | 0x15D | 0x3F | 87 | 0x6B | 0x8F | 148 | 0x95 | 0x00 |
27 | 0x160 | 0x7C | 88 | 0x6C | 0x44 | 149 | 0x96 | 0x00 |
28 | 0x161 | 0x3F | 89 | 0x57 | 0xDA | 150 | 0x97 | 0x00 |
29 | 0x164 | 0x7C | 90 | 0x57 | 0x9A | 151 | 0x9C | 0x00 |
30 | 0x165 | 0x4F | 91 | 0x57 | 0x1A | 152 | 0x57 | 0x1A |
31 | 0x16C | 0x7C | 92 | 0x58 | 0x3E | 153 | 0x57 | 0x3A |
32 | 0x1B0 | 0x1C | 93 | 0x58 | 0x3C | 154 | 0x57 | 0x7A |
33 | 0x1B1 | 0x5F | 94 | 0x58 | 0x38 | 155 | 0x57 | 0xFA |
34 | 0x1D8 | 0x1C | 95 | 0x58 | 0x30 | 156 | 0x58 | 0x01 |
35 | 0x1D9 | 0xAF | 96 | 0x58 | 0x20 | 157 | 0x58 | 0x03 |
36 | 0xB2 | 0x1F | 97 | 0x58 | 0x00 | 158 | 0x58 | 0x07 |
37 | 0xB5 | 0x7F | 98 | 0x89 | 0x20 | 159 | 0x58 | 0x0F |
38 | 0x165 | 0xFF | 99 | 0x95 | 0x00 | 160 | 0x58 | 0x1F |
39 | 0x38 | 0x01 | 100 | 0x96 | 0x00 | 161 | 0x58 | 0x3F |
40 | 0xA4 | 0x30 | 101 | 0x97 | 0x10 | 162 | 0x45 | 0x8A |
41 | 0xC5 | 0x7F | 102 | 0x9C | 0x00 | 163 | 0x45 | 0x0A |
42 | 0xA8 | 0x00 | 103 | 0x57 | 0x1E | 164 | Delay 1.3 x 3 GSPS/ FS seconds | |
43 | 0xA2 | 0x63 | 104 | 0xFE | 0x20 | 165 | 0x47 | 0xC0 |
44 | 0xA3 | 0x00 | 105 | 0xFF | 0x19 | 166 | 0x46 | 0x03 |
45 | 0xAD | 0x02 | 106 | 0x46 | 0x02 | 167 | 0x47 | 0xC0 |
46 | 0x05 | 0x80 | 107 | 0x45 | 0x8A | 168 | 0x05 | 0x80 |
47 | 0x20 | 0x1F | 108 | 0x45 | 0x0A | 169 | 0x20 | 0x1F |
48 | 0x93 | 0x20 | 109 | Delay 1.3 x 3 GSPS/ FS seconds | 170 | 0x9D | 0x05 | |
49 | 0x20 | 0x00 | 110 | 0x05 | 0x80 | 171 | 0x9E | 0x08 |
50 | 0x05 | 0x00 | 111 | 0x04 | 0x01 | 172 | 0x8B | 0x40 |
51 | 0x04 | 0x01 | 112 | 0x20 | 0x1F | 173 | 0x20 | 0x00 |
52 | 0x20 | 0x1F | 113 | 0x82 | 0x00 | 174 | 0x05 | 0x00 |
53 | 0x93 | 0x20 | 114 | 0x9D | 0x05 | 175 | 0x04 | 0x01 |
54 | 0x04 | 0x01 | 115 | 0x9E | 0x08 | 176 | 0x20 | 0x1F |
55 | 0x20 | 0x00 | 116 | 0x9D | 0x45 | 177 | 0x9D | 0x05 |
56 | 0x04 | 0x00 | 117 | 0x9D | 0x05 | 178 | 0x9E | 0x08 |
57 | 0x05 | 0x20 | 118 | 0xA0 | 0x80 | 179 | 0x8B | 0x40 |
58 | 0xC0 | 0x7C | 119 | 0xA2 | 0x80 | 180 | 0x20 | 0x00 |
59 | 0xBC | 0x3C | 120 | 0xA4 | 0x80 | 181 | 0x04 | 0x00 |
60 | 0xC9 | 0x01 | 121 | 0xA6 | 0x80 | |||
61 | 0xC9 | 0x00 | 122 | 0xA8 | 0x80 |