JAJSLC0 March 2024 ADC3683-SP
PRODMIX
In this mode, both the current and the previous sample have to be used in the address space as shown in Figure 7-40. The address order is different for 14/18-bit and 16/20-bit. Note: there are unused addresses between samples for resolution less than 20-bit (gray back ground), which can be skipped if not used.
In the following example (Figure 7-41), the 16-bit 2-wire serial output is reordered to where lane DA1/DB1 carries the 8 MSB and lane DA0/DB0 carries 8 LSBs.