JAJSGE8B March 2016 – October 2018 ADS1282-SP
PRODUCTION DATA.
Figure 80 shows the digital connection to a field programmable gate array (FPGA) device. In this example, two ADS1282-SP devices are shown connected. The DRDY output from each ADS1282-SP device can be used; however, when the devices are synchronized, the DRDY output from only one device is sufficient. A shared SCLK line between the devices is optional.
NOINDENT:
NOTE: Dashed line is optional.