JAJSGE8B March 2016 – October 2018 ADS1282-SP
PRODUCTION DATA.
The last stage of the ADS1282-SP filter block is a first-order HPF implemented as an IIR structure. This filter stage blocks DC signals and rolls off low-frequency components below the cut-off frequency. The transfer function for the filter is shown in Equation 17 of the デバイス・サポート.
The high-pass corner frequency is programmed by registers HPF[1:0], in hexadecimal. Equation 10 is used to set the high-pass corner frequency. Table 8 lists example values for the high-pass filter.
where
ƒHP (Hz) | DATA RATE (SPS) | HPF[1:0] |
---|---|---|
0.5 | 250 | 0337h |
1 | 500 | 0337h |
1 | 1000 | 019Ah |
The HPF causes a small gain error, in which case the magnitude of the error depends on the ratio of ƒHP/ƒDATA. For many common values of (ƒHP/ƒDATA), the gain error is negligible. Figure 44 shows the gain error of the HPF. The gain error factor is illustrated in Equation 16 (see デバイス・サポート).
Figure 45 shows the first-order amplitude and phase response of the HPF. In the case of applying step inputs or synchronizing, the settling time of the filter should be taken into account.