JAJSGE8B March 2016 – October 2018 ADS1282-SP
PRODUCTION DATA.
This command is used to exit the standby mode. Upon sending the command, the time for the first data to be ready is illustrated in Figure 49 and Table 9. Sending this command during normal operation has no effect; for example, reading data by the Read Data Continuous method with DIN held low.