JAJSPC7A December 2022 – August 2023 ADS131B23
PRODUCTION DATA
Offset drift is defined as the change in offset voltage over the specified temperature range. Offset drift is calculated using the box method in which a box is formed over the maximum and minimum offset voltages and over the specified temperature range. The box method specifies limits for the temperature error but does not specify the exact shape and slope of the device under test. For that reason, offset drift is specified as a positive number only, even though the drift can possibly be negative. Equation 1 shows the offset drift calculation using the box method:
where: