JAJSDZ9 October 2017 ADS54J64
PRODUCTION DATA.
The internal registers of the ADS54J64 can be programmed (as shown in Figure 74) by:
The ADS54J64 has several different register pages (page selection in address 11h, 12h). Specify the register page before writing to the desired address. The register page only must be set one time for continuous writes to the same page.
During the write operation, the SDOUT pin is in a high-impedance mode and must float.