The content from one of the two analog banks can be read out by:
- Drive the SEN pin low.
- Select the page address of the register whose content must be read.
- Master page: write address 0011h with 80h.
- ADC page: write address 0011h with 0Fh.
- Set the R/W bit to 1 and write the address to be read back.
- Read back the register content on the SDOUT pin, as shown in Figure 7-21. When a page is selected, multiple read backs from the same page can be done.