Use a solid ground plane underneath the device and partition the PCB into analog and digital sections.
Avoid crossing digital lines with the analog signal path and keep the analog input signals and the reference input signals away from noise sources.
The power sources to the device must be clean and well-bypassed. Use
CAVDD decoupling capacitors in close proximity to the analog
(AVDD) power-supply pin.
Use a CDVDD decoupling capacitor close to the digital (DVDD) power-supply pin.
Avoid placing vias between the AVDD and DVDD pins and the bypass capacitors.
Connect the ground pin to the ground plane using a short, low-impedance path.
Also connect the thermal pad to the ground plane.
Place the charge kickback filter components close to the device.
Among ceramic surface-mount capacitors, COG (NPO) ceramic capacitors are recommended because these components provide the most stable electrical properties over voltage, frequency, and temperature changes.
Figure 8-10 shows the typical connection diagram of the ADS7142-Q1.