JAJSH04C May 2013 – March 2019 ADS8866
PRODUCTION DATA.
As shown in Figure 39, the device features a single-ended analog input. AINP can swing from GND – 0.1 V to VREF + 0.1 V and AINN can swing from GND – 0.1 V to GND + 0.1 V. Both positive and negative inputs are individually sampled on 55-pF sampling capacitors and the device converts for the voltage difference between the two sampled values: VINP – VINN. The single-ended signal range is 0 V to VREF.
Figure 40 shows an equivalent circuit of the input sampling stage. The sampling switch is represented by a 96-Ω resistance in series with the ideal switch; see the ADC Input Driver section for more details on the recommended driving circuits.
Figure 40. Input Sampling Stage Equivalent Circuit Figure 39 and Figure 40 illustrate electrostatic discharge (ESD) protection diodes to REF and GND from both analog inputs. Make sure that these diodes do not turn on by keeping the analog inputs within the specified range.