JAJSP59B January 2023 – May 2024 ADS9218 , ADS9219
PRODMIX
The ADS921x has a precision, low-drift voltage reference internal to the device. For best performance, the internal reference noise is filtered (as shown in Figure 6-2) by connecting a 10µF ceramic bypass capacitor to the REFIO pin. As shown in Figure 6-3, an external reference is also connected at the REFIO pin. When using an external reference, disable the internal reference voltage by either of the following two options: