The ADC outputs digital ramp values
with increments specified in the RAMP_INC_A and RAMP_INC_B registers in place of ADC
A and ADC B data, respectively.
- Configure the increment value
between two successive steps of the digital ramp in the RAMP_INC_A (address
= 0x13) and RAMP_INC_B (address = 0x18) registers, respectively. The digital
ramp increments by N + 1, where N is the value configured in these
registers.
- Set TP_EN_A = 1, TP_MODE_A =
2 (address = 0x13), TP_EN_B = 1, and TP_MODE_B = 2 (address = 0x18)