JAJSTM8 April 2024 AFE20408
PRODUCTION DATA
The device integrates a low-pass digital filter that performs both decimation and filtering on the ADC output data, which helps with noise reduction. The digital filter is automatically adjusted for the different output data rates and always settles within one conversion cycle. The user has the flexibility to choose different output conversion time periods (TCT) from 52µs to 4.122ms. With this configuration the first amplitude notch appears at the Nyquist frequency of the output signal which is determined by the selected conversion time period and defined as fNOTCH= 1 / (2 × TCT). This means that the filter cut-off frequency scales proportionally with the data output rate. Figure 6-5 shows the filter response when the 1.054ms conversion time period is selected
Conversion time = 1.054ms, single conversion only |