SBFS042 June 2020 AFE3010
PRODUCTION DATA.
The following procedure details how to design a GFCI system with the AFE3010. The procedure is not intended to represent all of the validation required for a GFCI system to comply with the necessary regulations. The main goals are to tune the ground fault trip level and neutral-to-ground (N-G) detection of the system.
Table 5 presents the key parameters needed for the components in Figure 15. Table 5 also provides brief explanations of components and parameters. Component voltage ratings are dependent upon either the 20-V internal shunt regulator, the internal 5-V rail, or by the line voltage itself. Note that while Table 5 shows tested and working values, some components could be optimized further to reduce necessary power and voltage ratings depending upon the system requirements.
| COMPONENT DESIGNATOR | COMPONENT VALUE | COMPONENT RATINGS | DESCRIPTION |
|---|---|---|---|
| C1 | 3.3 µF | 50 V, ±10%, X7R | Primary decoupling capacitance for AFE3010. Voltage rating dependent upon the 20-V shunt regulator. |
| C2 | 0.1 µF | 50 V, ±10%, NP0 | Capacitive load for NG_OUT driver to generate a current pulse. Voltage rating dependent upon the 20-V shunt regulator. |
| C3 | 0.47 µF | > 5 V, ±10%, X7R | Tunes and stabilizes the amplifier response so VOUT is inverted with Line at normal polarity. |
| C4 | 1 nF | > 5 V, ±10%, NP0 | Improves the noise immunity of the amplifier and comparators. TI does not recommend to increase this value further. |
| C5 | 1 nF | > 5 V, ±10%, NP0 | Improves the noise immunity of the amplifier. It can be increased up to 150 nF given R6 and R7 do not change. Always check for amplifier stability over-temperature when increasing this value. |
| C6 | 180 pF | > 5 V, ±10%, NP0 | It helps keep the reference voltage buffer stable from high-frequency noise transients. TI does not recommend to increase this value further. |
| C7, C8, C9 | 1 nF | > 5 V, ±10%, NP0 | These capacitors filter noise coupled to their respective digital pins. |
| C10 | 0.47 µF | > 5 V, ±10%, X7R | These capacitors help prevent noise coupling into the gate of the SCR. |
| C11 | 2 .2 nF | 250 VAC, ±10%, X7R | Helps keep the SCR anode stable. Voltage rating dependent upon line voltage. |
| D1 | N/A | 600 V, 1 A | Provides line voltage rectification for AFE3010 VDD. Voltage rating dependent upon line voltage. |
| D2 | N/A | 1000 V, 1 A | Provides current rectification for SCR and solenoid. Voltage rating dependent upon line voltage. |
| D3 | Red | Red LED | LED driven by ALARM to indicate initial passing of self-test on power up and self-test failure. |
| D4 | N/A | 600 V, 1 A | Prevents any current flowing from emitter to collector in Q1, which protects the AFE3010 from current injection during abnormal states of Q1. |
| Q1 | 400 V | 400 V, 1 A | NPN transistor controlled by FT driver to perform periodic self-tests. |
| R1, R2, R3, R4 | 18.0 kΩ | 5%, 0.5 W | Limit current for AFE3010 shunt regulator at VDD. Resistors are placed in two parallel pairs to ensure normal operation even if a resistor fails. One pair is placed above the bridge (D1) to limit current in event of a D1 failure. Power rating determined by line voltage and supply current. |
| R5 | 100 Ω | 1%, 0.1 W | Limits current into NG_OUT pin during inductive kickback from driving 200-turn coil. Limiting the current will keep the internal ESD cells from turning on and potentially damaging the device. Thus, take caution when decreasing this value to improve N-G detection. To reduce R5 and protect AFE3010, a Schottky diode can be used at NG_OUT to clamp pin voltage during inductive kickback. |
| R6 | 75 Ω | 1%, 0.1 W | Input resistor for the internal amplifier. R6 can be adjusted to improve N-G detection. |
| R7 | 36 kΩ | 1%, 0.1 W | Feedback resistor for the internal amplifier. Sets the gain for ground fault signals. Thus, R7 can be adjusted to change the device trip point. |
| R8 | 10.5 kΩ | 1%, 0.5 W | Sets the level of fault current used in the periodic self-test when Q1 is turned on. The fault current should be greater than the trip point for successful detection and operation. The self-test will be hardest to pass when line connects to GFCI with reverse polarity and there is a small leakage current that is below the trip current. The worst-case power condition will be when a device cannot detect the self-test fault current and thus Q1 is on for a half-cycle of line. |
| R9 | 1.5 kΩ | 5%, 0.1 W | Limits the output current of the ALARM driver. Using a higher R9 value will reduce supply current when ALARM is driving D3. |
| R10 | 560 Ω | 5%, 0.1 W | Limits the output current of the SCR driver. |
| R11 | 51 kΩ | 5%, 1/3 W | Limits the current into the SCR_TST pin when regulating to 20 V and sets internal biasing. The value of the resistor should not change from the recommendation when SEL = LOW. The lowest acceptable value is a 1% 49.9 kΩ. Given a 170-V peak line voltage, the average power rating required is calculated with [((170 V – 20 V)2) /R11] / [2 × SQRT(2)]. |
| R12 | 1 MΩ | 5%, 0.1 W | Limits the current into PH pin. |
WARNING
When evaluating this device, implement high-voltage safety precaution and procedures.
Figure 16. Neutral-to-Ground Detection Test Setup for AFE3010 Design Procedure