SPRSPB0 December 2024 AM2754-Q1
ADVANCE INFORMATION
The device has three instances of the GPIO module.
GPIOn_x is generic name used to describe a GPIO signal, where n represents the specific GPIO module and x represents one of the input/output signals associated with the module.
For more information, see General-Purpose Interface (GPIO) section in Peripherals chapter in the device TRM.