SBASAY6 December 2024 AMC0236
PRODUCTION DATA
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
Do not leave the analog input (INP pin) of the AMC0x36 unconnected when the device is powered up. If the device input is left floating, the output of the device is not valid.
Do not connect protection diodes to the input (INP pin) of the AMC0x36. Diode leakage current potentially introduces significant measurement error especially at high temperatures. The input pin is protected against high voltages by the ESD protection circuit and the high impedance of the external resistive divider.