JAJSPV9 December 2024 AMC0386
PRODUCTION DATA
The resistive divider at the input of the AMC0386 scales down the voltage applied to the HVIN pin to a ±1V linear full-scale level. This signal is available on the SNSP pin, which is also the input of the analog signal chain.
The high-impedance input buffer on the SNSP pin feeds a second-order, switched-capacitor, feed-forward ΔΣ modulator. The modulator converts the analog signal into a bitstream that is transferred across the isolation barrier, as described in the Isolation Channel Signal Transmission section.
For reduced offset and offset drift, the input buffer is chopper-stabilized with the chopping frequency set at fCLKIN/16. Figure 7-1 shows the spur at 625 kHz that is generated by the chopping frequency for a modulator clock of 10 MHz.
sinc3 filter, OSR = 1, fCLKIN = 10MHz, fIN = 1kHz |