As shown in Figure 8-29, the AMC131M02 has two internal data buffers per ADC channel holding
conversion data: an ADC output buffer and a FIFO buffer. Each buffer can only
hold one conversion result at a time. The data output on DOUT is always from the FIFO
buffer.
Whenever an ADC channel generates new conversion data, the ADC output
buffer for that channel is
updated immediately with the new data. However, updating the FIFO buffer depends on the
previous conversion data retrieval by the host. There are three scenarios:
- If conversion data (N) stored in the FIFO
buffer has already been read by the host at the time that new conversion data (N+1) become
available, then the FIFO buffer is updated with the new conversion data (N+1). In this
case, data in both the ADC output buffer and the FIFO buffer are updated at the same time
(that is, both buffers now hold the same conversion data N+1).
- If conversion data (N) stored in the FIFO
buffer has not yet been read by the host when new conversion data (N+1) become
available, then the FIFO buffer is not updated and still holds the previous
conversion data (N), while the ADC output buffer now holds the new conversion data (N+1).
In this case, data content is different between the ADC output buffer (N+1) and the FIFO
buffer (N). After the host reads conversion data N from the FIFO buffer, the FIFO buffer
is updated with the conversion data N+1. The host can then retrieve conversion data
N+1.
- A special scenario exists if conversion data (N) stored in the FIFO
buffer has not been read by the host, but two new conversion data already
became available in the meantime (that is, the ADC output buffer is updated with
conversion data N+2). In this case, the FIFO buffer is updated with conversion result N+2
at the same time the ADC output buffer is updated with conversion result N+2 (that is,
both buffers now hold the same conversion data N+2). That means, conversion data N and N+1
are lost and cannot be retrieved by the host anymore.
Table 8-12 summarizes the ADC output buffer and FIFO buffer operation when new conversion data (N+1)
are available.
Table 8-12 New Conversion Data Available:
Operation of the ADC Output Buffer and FIFO Buffer
SPI HISTORY |
NEW CONVERSION DATA AVAILABLE AT TIME
t = tS |
ADC OUTPUT BUFFER CONTENT
(t < tS) |
FIFO BUFFER CONTENT
(t < tS) |
ADC OUTPUT BUFFER CONTENT
(t > tS) |
FIFO BUFFER CONTENT
(t > tS) |
FIFO data N has been read by the host |
N+1 |
N |
N |
N+1 |
N+1 |
FIFO data N has not yet been read by the
host |
N+1 |
N |
N |
N+1 |
N |
FIFO data N has not yet been read by the
host |
N+2 |
N+1 |
N |
N+2 |
N+2 |
The following three examples illustrate the
behavior of the ADC output and FIFO buffer using a simplified notation to indicate which
conversion data is stored in each buffer: [number of sample in the ADC output buffer |
number of sample in the FIFO buffer].
Example 1: Host reads conversion results
as soon as the results become available
- When the first conversion (result 1)
completes, this result is placed both in the ADC output buffer and the FIFO buffer [1 |
1].
- If the host reads conversion result 1
immediately after the conversion completes, the content of the buffers stays at [1 | 1].
The host can read conversion result 1 from the FIFO buffer multiple times if needed before
conversion result 2 completes.
- When conversion result 2 completes, the
result is again placed into both the ADC output buffer and the FIFO buffer [2 | 2].
- If the host reads the result before the
third conversion completes, result 2 is read out and the buffers stay at [2 | 2].
Example 2: Host misses reading one
conversion result
- When the first conversion (result 1)
completes, the result is placed both in the ADC output buffer and the FIFO buffer [1 |
1].
- If the host misses reading result 1 from
the FIFO buffer before the second conversion completes, then the ADC output buffer holds
result 2, and the FIFO buffer still holds result 1 [2 | 1].
- If the host now reads data before the
third conversion completes, result 1 is read. The content of the buffers then updates to
[2 | 2].
- Another conversion data read request by
the host shifts out result 2 on DOUT. The buffers stay at [2 | 2].
- Now when the third conversion completes,
both buffers update with result 3 [3 | 3].
Example 3: Host misses reading two
consecutive conversion results
- When the first conversion (result 1)
completes, the result is placed both in the ADC output buffer and the FIFO buffer [1 |
1].
- If the host misses reading result 1 from
the FIFO buffer before the second conversion completes, then the ADC output buffer holds
result 2, and the FIFO buffer still holds result 1 [2 | 1].
- Now if the third conversion completes and
the host still did not retrieve data from the FIFO buffer, then result 3 overwrites the
data in both the ADC output and FIFO buffer [3 | 3].
- In this case, both conversion result 1
and result 2 are lost and cannot be read anymore by the host.
Resulting from the internal structure of the
ADC, including the ADC output buffer and the FIFO buffer, the DRDY pin
behaves as described:
- If conversion data are read by the host
every time new conversion data become available, then DRDY follows
the format described in the Data Ready (DRDY) section, depending on the DRDY_FMT bit in the MODE register: When the DRDY_FMT
bit is 0b, new data are indicated by DRDY changing from high to low
and remaining low until either all conversion data are shifted out of the device, or
remaining low and going high briefly before the next time DRDY
transitions low. When the DRDY_FMT bit is 1b, new data are indicated by a short negative
pulse on the DRDY pin.
- If the DRDY_FMT bit is 0b and the host
does not read conversion data from the FIFO buffer before the next conversion completes,
then DRDY remains low and goes high briefly before the next time
DRDY transitions low (indicating a new conversion).
- If the DRDY_FMT bit is 1b and the host
does not read conversion data from the FIFO buffer before the next conversion completes,
then the device skips one DRDY pulse and does not provide another
DRDY pulse until the second following instance when data are
ready. Therefore, if the DRDY_FMT bit is 1b and the host does not read conversion data
at all, the DRDY pin toggles at a rate which is half the conversion
rate.