JAJSOY8H November 2011 – July 2022 BQ24160 , BQ24160A , BQ24161 , BQ24161B , BQ24163 , BQ24168
PRODUCTION DATA
In order for charging to occur, the source voltage as measured at the IC's USB or IN pins (factoring in cable/trace losses from the source) must be greater than the VINDPM threshold (but less than the maximum values above) and the source's current rating must be higher than the buck converter needs to provide the load on SYS. For charging at a desired charge current of ICHRG, VUSBorINx IUSBorIN x η > VSYS x (ISYS+ ICHRG) where η is the efficiency estimate from Figure 7-1 or Figure 7-2 and VSYS = VBAT when VBAT charges above VMINSYS. The charger limits IUSBorIN to that input's current limit setting. With ISYS = 0 A, the charger consumes maximum power at the end of CC mode, when the voltage at the BAT pin is near VBATREG but ICHRG has not started to taper off toward ITERM.