SLUS763D July 2007 – April 2016
PRODUCTION DATA.
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
In some applications, the equipment that the protection IC resides in may be required to provide power to an accessory (for example, a cellphone may power a headset or an external memory card) through the same connector pins that are used by the adapter for charging. Figure 24 and Figure 25 illustrate typical charging and accessory-powering scenarios:
In the second case, when power is being delivered to an accessory, the bq24314 and bq24316 devices are required to support current flow from the OUT pin to the IN pin.
If VOUT > VUVLO + 0.7 V, FET Q1 is turned on, and the reverse current does not flow through the diode but through Q1 (see Figure 26). Q1 will then remain ON as long as VOUT > VUVLO – VHYS-UVLO + RDSON × IACCESSORY. Within this voltage range, the reverse current capability is the same as the forward capability, 1.5 A.
NOTE
There is no overcurrent protection in this direction.