JAJSDT4C May 2017 – September 2021 BQ25606
PRODUCTION DATA
After REGN LDO powers up, the device confirms the current capability of the input source. The input source must meet both of the following requirements in order to start the buck converter.
If the device fails the poor source detection, it repeats poor source qualification every 2 seconds.