JAJSQM7B June 2023 – February 2024 BQ25628E
PRODUCTION DATA
After the REGN LDO powers up, the device checks the current capability of the input source. The input source has to meet the following requirements in order to move forward to the next power on steps.
Once these conditions are met, the device proceeds to input source type detection.