SLUS696C June 2006 – February 2019
PRODUCTION DATA.
The SHA-1 is known as a one-way hash function, meaning there is no known mathematical method of computing the input given only the output. The specification of the SHA-1, as defined by FIPS 180-2, states that the input consists of 512 bit blocks with a total input length less than 264 bits. Inputs which do not conform to integer multiples of 512 bit blocks are padded before any block is input to the hash function. The SHA-1 algorithm outputs 160 bits, commonly referred to as the digest.
The full SHA-1 specification and algorithm can be found at http://csrc.nist.gov/publications/fips under FIPS 180. (As of April 23, 2004, the latest revision is FIPS 180-2.)
The bq26100 device generates an SHA-1 input block of 288 bits (total input = 160 bit message + 128 bit key). To complete the 512 bit block size requirement of the SHA-1, the bq26100 device pads the key and message with a 1, followed by 159 0’s, followed by the 64 bit value for 288 (000…00100100000), which conforms to the pad requirements specified by FIPS 180-2 9 (Figure 17).