JAJSFF8E October 2012 – May 2018
PRODUCTION DATA.
The bq27545-G1 can indicate tab disconnection by detecting change of StateOfHealth(). This feature is enabled by setting [SE_TDD] bit in Pack Configuration B. The [TDD] of Flags() is set when the ratio of current StateOfHealth() divided by the previous StateOfHealth() reported is less than TDD SOH Percent. The [TDD] of Flags() can be configured to control an interrupt pin (SE or HDQ) by enabling INTERRUPT mode. Refer to INTERRUPT Mode for details.