JAJSFF8E October 2012 – May 2018
PRODUCTION DATA.
SLEEP mode is entered automatically if the feature is enabled (Pack Configuration [SLEEP]) = 1) and AverageCurrent() is below the programmable level Sleep Current. Once entry into SLEEP mode has been qualified, but before entering it, the bq27545-G1 performs an ADC autocalibration to minimize offset.
While in SLEEP mode, the fuel gauge can suspend serial communications as much as 4 ms by holding the comm line(s) low. This delay is necessary to correctly process host communication, because the fuel gauge processor is mostly halted in SLEEP mode.
During the SLEEP mode, the bq27545-G1 periodically takes data measurements and updates its data set. However, a majority of its time is spent in an idle condition.
The bq27545-G1 exits SLEEP if any entry condition is broken, specifically when (1) AverageCurrent() rises above Sleep Current, or (2) a current in excess of IWAKE through RSENSE is detected when the Iwake comparator is enabled.