JAJSHO8T November 2013 – August 2022 BQ2961 , BQ2962
PRODMIX
The UNDERVOLTAGE mode is detected if any of the cell voltage across (V1–VSS), (V2–V1), (V3–V2), or (V4–V3) is below the VUVREG threshold for tUV_DELAY time. In this mode, the regulated output is disabled. To return to the NORMAL mode, all the cell voltages must be above (VUVREG + VUVHYS).
For a low cell configuration, Vn pin can be shorted to the (Vn – 1) pin. The device ignores any differential cell voltage below VUVQUAL threshold for undervoltage detection.